Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is an CFF fault on the ATV58 drives?
Issue:
CFF fault on ATV58.

Product Line:

Altivar ATV58

Environment:
All

Cause:
Error probably caused by changing a card.

Resolution:
There are four CFF fault messages to troubleshoot.

-PWR RAT ERR-ENT:Change on the power board ratings, maybe someone changed out the power board.

-Option ERR, -ENT: Option board changed or they installed a new option board.

-Opt. Remove-ENT: Option card was removed.

-EEP CKS,-ENT: Saved configuration cannot be read. ENT button will prompt you to do a factory reset.

Other troubleshooting tips:

Check the J connections between the main control board and power board to see if they are loose or disconnected.

Reset the drive back to a factory default.

Check cooling fans to see if they are running. You might get CFF if the cooling fans are bad too. Just check them.

Reference manual VVDED397047USR8/02 page 96.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings