Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HU365R, Series E5 (or E05) heavy duty safety switch?
Issue:
Current design repair parts

Product Line:
Heavy Duty Safey Switch

Resolution:
The parts listed here are the only field replaceable parts.
LIne/Load base assembly  -  4055218951 (3 required; includes arc suppressor assembly)
Arc suppressor assembly - 4051270850 (3 required)
Main Lug assembly - 4025113650 (2 required per base assembly)
Line base phase insulator - 4055219301 (2 required)
Line base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217251 (also recommend replacing handle gasket, part number 4051126101)
Handle knob kit - 4028343550
Door thumb screw and retainer - 4405043401 (screw) and 4405043301 (retainer)
Long Cross Bar Insulator - 4055217801
Short cross bar insulators - 4055217701 (2 required)
Dust shield - 4055215701

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings