Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the QO200TR be padlocked in the ON or OFF position?
Issue:
Locking the QO200TR in the ON or OFF position

Product Line:
Air Conditioner Disconnect

Resolution:
The cover of the enclosure can be padlocked closed, but a padlock attachment cannot be used with the enclosed molded case switch. The enclosure is too small for the cover to be installed when a padlock attachment is attached to the enclosed molded case switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings