Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are ground detection lamps available for panelboards?

Issue:
Ground detection lamps for Panelboards

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 29 & 94-1989, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1

Cause:
Ground detection lamps annunciate the unintended grounding of an ungrounded electrical distribution system.

Resolution:
Ground detection lamps are available only for I-Line panelboards.  A TAG adder and factory review of the panelboard is required, as enclosure modifications will likely be necessary to accommodate this feature.  The NQ and NF enclosures cannot accommodate this feature.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings