Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Replacement connectors for Powerlink G3 Controllers
Issue:
Customer needs replacement connectors ( terminals ) for Powerlink G3 Controllers

Product Line:
Powerlink G3

Environment:
NF500GE, NF1000G3, NF2000G3, NF3000G3, NF3000G3C

Cause:
Customer lost the original pack of connectors that were included with the G3 controller when controller or panel was originally purchased.

Resolution:
G3 Hardware Pack is part number 63249-401-29.  It contains a connector for each of the I/O terminal on a G3 Controller:  8 3-Pin Connectors,  1 5-Pin Connector,  1 2-Pin Connector.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings