Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How can one add two QOB360 or similar amp breakers across from each other in an old NQOB panel using the hex head standoffs in a SK5668 kit?

Issue:
Adding 3p breakers to an NQOB using the SK5668 kit

Product Line:
Panelboards

Environment:
NQOB

Cause:
Mounting

Resolution:
The kit has A, B and C phase connectors and screws and the A & C are symmetric.  The latest version with hex head B phase connectors is very difficult to install if not impossible.  Due to the close proximity of the plastic insulators on either side of the connectors, there is no room for a wrench or nut driver.

Perhaps by inserting a screw into the top of each B phase connector, they can be slowly driven into position.  Turn one hex head standoff 1/4 turn, then the other 1/4 turn, and repeat the process until they are both tight.  Then install both breakers together.  Here are the directions written on the envelope of the SK5668:

Replacing the interior with an NQ in the existing box or a complete panel changeout to a new NQ package is most likely the best choice.  Another option is to find an old SK5668 with round standoffs.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings