Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the vertical and end trim piece part numbers for a complete HCW59TS 4 piece trim. What are the trim pieces for the I Line 4 piece trim part number HCW59TS?

Issue:
What are the vertical and end trim piece part numbers for a complete HCW59TS 4 piece trim

Product Line:
I Line panelboards

Environment:
Trim pieces for the I Line 4 piece trim part number HCW59TS

Cause:
Replacement trim pieces for lost, or damaged trim parts

Resolution:
The (2) vertical trim part number is 80104-250-10,. The Top and Bottom horizontal end trim part number is 80104-888-50

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings