Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
NF1000G3 zone AND logic not working
Issue:
NF1000G3 with a schedule and input controlling the zone. With the zone logic set to AND, and the input sync to the schedule the input turns the zone on during the off time of the schedule.

Product Line:
Powerlink
Powerlink G3
G3
NF1000
NF1000G3
1000

Environment:
When using a NF1000G3 with a schedule and a input to control the zone. The zone AND logic does not work after the schedule turns off, the zone turns on with the input even with the zone logic set to AND. When setting up the input sync and setting it to events from the schedule the AND logic does not work as it should.

Cause:
The NF1000G3 reverts the zone logic to a OR when the input is sync to a event of the schedule.

Resolution:
Do not use the input sync to the schedule.
Set the input as a Time ON for 1 second.
Inhibit the timer of the input during the schedule.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings