Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What main breaker should be used with a NQ42L2 ?

Issue:
Part number of the main breaker for the NQ42L2

Product Line:
Panelboards

Environment:
NQ single phase

Resolution:
Use a QBL32100 with a NQMB2Q or HDL36100 or JDL26150 with a NQMBHJ or similar 3 pole breaker per the * footnote on p. 9-7 of the digest 176. The B phase lug on the breaker can be removed to avoid confusion. The bus links on the outer poles of the adapter kit and the deadfront cutout only works with 3p breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings