Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What ground bar kit is used for the HOM612L100S, HOM612L100F, and HOM612L100RB load centers?

Issue:
Product Design Features

Product Line:
Load Center

Resolution:
The ground bar kit is catalog number PK7GTA and is required when the load centers are used as a sub panel. It must be ordered separately from the load center.
HOM612L100F
Installation instructions for the PK7GTA can be found here.

More information on Load Centers can be found by visiting - Load Centers.

Schneider Electric USA

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings