Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can I change the date and the time on an ATV61 Drive?
Issue:
ATV61 time and date modification

Product Line:
Altivar 61 Altivar 71 ATV61  ATV71

Environment;
All

Cause:
Used typically for Time and Date stamp  in Fault History

Resolution:
IMC Option Card VW3A3521S0  or CIC Card VW3A3501 allow you to set the date and time in the drive, even if you're not controlling from the card.  You set this in Menu 1.14 in the Drive Menu.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings