Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can I setup Powerlink Remote Source over RS-485 Serial network?
Issue:
How do I setup Powerlink Remote Source over RS-485 Serial network?

Product Line:
Powerlink G3/G4 Lighting Control Panels

Environment:
Powerlink G3/G4 Lighting Control Configuration

Cause:
Remote Sources allow an input on one Powerlink G3/G4 Controller to control actions on another Powerlink G3 controller.

Resolution:
Remote Source is only possible if the controllers are setup with an IP network.   Powerlink Controllers must be of the NF2000G3, NF3000G3, NF3000G3C, and NF3500G4 variety.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings