Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
PBQ4660G and Fuse Selection
Issue:
How many fuses does the PBQ4660G 600A busway plug accept?

Product Line:
I-Line Busway and Accessories

Environment:
Installation/Operation

Cause:
Selection of correct number of fuses.

Resolution:
This is a 3 phase device and will accept 3 fuses, Class H, K, or R fuses. It will also accept Class J fuses by moving the  load base assembly inside the switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings