Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do you set up the ATV61 drive to be used with the VW3A3314 Apogee P1 option card?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Resolution:
Card connector Pin outs

Contact B= (+) signal
Contact A= (-) signal
Contact GND= (GND)
Contact SCR= (Shield)

Programming Drive  ( You must Power cycle after changing any of the Menu 1.9 coms parameter settings)
Menu 1.9- Communications (CON)
Address range is 0-99  (Choose your address)
Baud rate: Choose between 4800 to 76800
Network time out = range is 2 to 60 seconds (Choose your network time out)

Menu 1.6 Command menu
Controlling the drive over the network
Ref 1 = Com card
Profile is Not separate
Point # 24 (LDO  table) is your start command for CMD  (writing a 1 will start 0 will stop)
Point # 60 (LAO table) is your input speed reference 1 in %
Note: If the drive will not start with writing a 1 to Point #24 try writing a 0 to #24 1st then writing a 1.

Reading data only from the drive.
Ref 1 AI1
Profile not separate
Point #03= freq output in hz
Point #05= speed output in rpms
Point # 06= Motor current
Point # 07= Motor Torque
Point # 08= Motor Power
Point # 09 = Drive Temp
There are other values that you can read in the LAI table see the attached document for information.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric USA

Attachment(s)
bbv10543-en.pdf [1.17 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings