Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a H465AWK, Series E4?
Issue:
Older design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218850 (4 required; arc suppressor assembly not included)
Load base assembly - 4055219050 (4 required)
Arc suppressor assembly - 4051270850 (4 required)
Line & Load base Lug assembly - 4025113650 (1 required per base assembly)
Keps nut for line & load base lug assembly - 2342702800 (1 required per lug)
Line base phase insulator - 4051201401 (3 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217251
Vault handle - 4051219450
Vault handle linkage assembly - 4051273650 (includes linkage assembly, (2) springs, (2) E-Clips, and (1) O-Ring)
Handle knob kit - 4028343550

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings