Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How to use Powerlink G3 as a modbus gateway
Issue:
How to use Powerlink G3 as a modbus gateway.
One can setup a Powerlink NF2000G3 or NF3000G3 on an ethernet network for Modbus over TCP/IP communications.  One can then wire up to 8 other devices by RS-485 communications from the 2-wire RS-485 terminals in the Powerlink G3.  Commands for the modbus devices can be sent over TCP/IP via the Powerlink G3 Controller.

Product Line:
Powerlink Lighting Control
NF2000G3, NF3000G3, NF3000G3C

Environment:
Powerlink G3 systems

Cause:
This feature allows devices to be accessed via modbus TCP/IP when then otherwise would require a direct modbus communication line back to the BAS network.

Resolution:
First setup the Powerlink G3 Controller for Modbus TCP/IP communications.   Set the modbus registers explained in the attached instruction bulletin to put the controller into Modbus Passthrough Mode.
Note that if the controller is an NF3000G3C with a C-bus network, then Modbus Passthrough Mode is not available.

Schneider Electric USA

Attachment(s)
Pass Through Mode.pdf [55.8 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings