Issue:
ATV61 and ATV71 Modbus and CANopen addresses
Product Line:
Altivar ATV61 and ATV71 modbus
Environment:
All
Cause:
Needs to find out the modbus address for Motor thermal, Drive thermal etc.
Resolution:
You can find the modbus and CANopen addresses in the
atv61_parameters_en and atv71_parameters_en comms manual.
Released for: Schneider Electric USA