Issue:
Current design repair parts
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the HU364N, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base - 4056703950 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Complete Line/Load Base mounting screws - 4020546401 (6 required per base)
Arc Suppressor Assembly - 4056677550 (1 required per phase; obsolete, no longer available, replaced by ASKE603)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025136550 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)
Released for: Schneider Electric USA