Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will an EDBPA / EDBPAF handle lock kit, work with a Series E1 EDB, NF panelboard breaker?
Issue:
EDBPA / EDBPAF handle lock kit will work with a Series E1 EDB breaker

Product Line:
NF Panelboard

Environment:
Accessories for Branch breakers

Cause:
Series E1 breakers will not accept current Series E2 and E3 EDB Breaker handle lock accessories

Resolution:
Due to the Series E1 breaker NOT having a slot in the upper portion of the breaker, the currently available Series E2, E3, EDPA and EDPAF handle lock kits will NOT work .
Replace breakers with either Series E2, or E3 breakers if accessory needed. See picture showing SLOT in the new Serie(s) Breakers below.


E Frame Breakers Slot

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings