Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the same end caps (EZMCAP or EZMSCAP) used, regardless of whether the EZM lineup is single phase or three phase?
Issue:
Product features

Product Line:
EZM

Resolution:
Yes, the EZMCAP would be used on the left and/or right side, and the EZMSCAP would be used on the right side only of the EZM device, regardless of it being single phase or three phase.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings