Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Powerlink G3 webpage on NF3000G3 controller has display errors on Internet Explorer 11
Issue:
Powerlink G3 webpage on NF3000G3 controller has display errors on Internet Explorer 11.   This error will occur on the Setup Tab of the page which is support to show a dynamic graphical representation of the Powerlink G3 controller LCD screen.

Product Line:
Powerlink Lighting Control

Environment:
Powerlink webpages

Cause:
The Powerlink G3 was developed in the early 2000's when Internet Explorer was at version 5,5.    Webpage technology and browsers have evolved over the years to the point where IE version 11 does not show the webpage correctly.

Resolution:
Sometimes websites don't look like you expect them to–images might not appear, menus might be out of place, and text could be jumbled together. This might be caused by a compatibility problem between Internet Explorer and the site you're on. Sometimes this can be fixed by adding the site to your Compatibility View list.

Click on the IE Tools icon
Click on Compatibility View Settings
Type in the IP of the Controller
Click Add then Close

Alternative solution is to use a different browser such as Google Chrome, Firefox, or Apple Safari

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings