Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is the EZM or Meter-Pak metering equipment available in free standing or floor mounted?
Issue:
Product Design

Product Line:
EZM and MP Metering

Resolution:
No, the EZM and MP metering equipment are ONLY available for wall mounting and are NOT available in free standing or floor mounted.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings