Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is 2441-D26-G13 limit arm?
Issue:
Customer has provided 2441-D26-G13 as part number, but this is not valid in the pricing system.  What is the correct part number?

Product Line:
9007 limit switches

Environment:
US Product

Cause:
2441-D26-G13 is an OEM part number and not used for general ordering.

Resolution:
This part number is for a 9007DA1 limit switch arm which is supplied without packaging.  For general ordering, use 9007DA1 to order individual quantities (these will come with packaging).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings