Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement 3 pole starter for an 8810SDO1?

Issue:
Need to replace the 3 pole starter in an 8810SDO1

Product Line:
8810 Two-Speed Starters

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The replacement will be 8536SDO1*


*add the appropriate voltage code on the end to make it a valid part number

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings