Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
6 hole enclosure for 22mm push buttons

Issue:

Is there a 22mm enclosure with 6 holes?

Product Line:

22mm XA enclosures

Environment:

US Product

Cause:

There is no 6 hole enclosure listed

Resolution:

There are no 6 hole enclosures for 22mm operators.  Can use XAPA2108 which an is 8 hole enclosure and plug two of the holes with ZB5SZ3 or similar plug.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings