Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
L1452M with 567 form code

Issue:

What is a L1452M567 limit switch?

Product Line:

RB Denison Lox limit switches

Environment:

US Product

Cause:

Form 567 is not listed in the Digest

Resolution:

The L1452M is an emergency (pull) stop type limit switch with 1 NC contact and maintained lever action.  The 567 form code added to this part number indicates a modification wherein the switch is potted with a two wire receptacle and epoxy sealed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings