Issue:
Per Section 110.22 of the NEC, equipment must be legibly marked in the field to indicate the equipment has been applied with a series combination rating. Schneider Electric provides a label for this purpose with all MP Meter-Pak™ meter centers and EZ Meter-Pak™ meter center branch devices, but it is a loose sticker and, if lost, the customer may need a replacement.
Resolution:
Order part number 4027337201. This will be one sheet with 8 series combination labels on it. See attachment for representative label.
Per Section 110.22 of the NEC, equipment must be legibly marked in the field to indicate the equipment has been applied with a series combination rating. Schneider Electric provides a label for this purpose with all MP Meter-Pak™ meter centers and EZ Meter-Pak™ meter center branch devices, but it is a loose sticker and, if lost, the customer may need a replacement.
Resolution:
Order part number 4027337201. This will be one sheet with 8 series combination labels on it. See attachment for representative label.
Released for: Schneider Electric USA