Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a lug for a 600A NQ panel that will accept (3) 250 kcmil Aluminum wire per phase
Issue:
Is there a lug for a 600A NQ panel that will accept (3) 250 kcmil Aluminum wire per phase

Product:
NQ panelboards sold and supported in the USA.

Environment;
Application

Cause:
Selection/product features

Resolution:
Order the NQALM6A lug kit. This kit contains three phase lugs, two neutral lugs and ten mounting screws.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings