Issue:
Product application
Product Line:
EZM Accessory
Resolution:
Yes, multiple bus extensions could be connected together. The 1 Phase Bus Extensions could be connected together, or the 3 Phase Bus Extensions could be connected together, but the 1 Phase and 3 Phase Bus Extensions cannot be used together. Each Bus Extension is secured to the wall independently (without the use of a Mounting Channel). They are not to be used for any other physical load bearing applications.
Product application
Product Line:
EZM Accessory
Resolution:
Yes, multiple bus extensions could be connected together. The 1 Phase Bus Extensions could be connected together, or the 3 Phase Bus Extensions could be connected together, but the 1 Phase and 3 Phase Bus Extensions cannot be used together. Each Bus Extension is secured to the wall independently (without the use of a Mounting Channel). They are not to be used for any other physical load bearing applications.