Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
8911DPS and NEMA 3R enclosure
Issue:
Do we offer a NEMA 3R enclosure for the 8911DPSO Definite Purpose Starters?

Product Line:
8911DPSO, Definite Purpose Starters

Environment:
8911 DPSO, 2 pole and 3 pole starters, 600VAC maximum

Cause:
What type enclsoures are available for the 8911DPSO procuct line?

Resolution:
No, only NEMA 1 enclosures are available for the 8911DPSO Definite Purpose Starters .

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings