Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the dimensions of the NC38FHR?
Issue:
Dimensions of NC38FHR hinged panel cover

Product Line:
NF Panelboards and Accessories

Environment:
NQ and NF panelboard covers

Resolution:
The dimensions for NC38FHR are 39.52 inches height and 21.52 inches width. The overhang is a total of 1.52 inches for the width and 1.52 inches total for the length.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings