Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What buzzers are available in the 22mm line of operators?

Issue:
Is there any continuous or intermittent buzzer on the 22 mm operators?

Product Line:
22mm push buttons

Environment:
Harmony XB5/ZB5 Plastic Push Buttons

Resolution:
There are two options,
XB5KSB is the 24Vac/Vdc buzzer
XB5KSG is the 120VAc buzzer
Units have 85 db buzzer:4kHz, continuous or intermittent

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings