Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Which 30mm operators are available with "Push Emergency Stop" printed directly on the knob?
Issue:
How to obtain a red knob with "Push Emergency Stop" printed on the red knob?

Product Line:
Push Buttons and Operator Interface

Environment:
30mm operators - GIC Product

Cause:
It can be helpful to have the knob pre-printed instead of purchasing a separate legend

Resolution:
Only the following E-stop button types are available with "Push Emergency Stop" printed on the knob:
9001KR4, 9001SKR4
9001KR5, 9001SKR5
9001KR8, 9001SKR8
9001KR9, 9001SKR9

Substitute "R05" in place of "R"
Ex. 9001KR9R05 instead of 9001KR9R

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings