Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the door kit for the HOM60120M200PC and HOM60120L225PC?
ISSUE:
Product Accessory

PRODUCT LINE:
Homeline Load Centers

RESOLUTION:
The part number for the door kit is QOCDK60.
NOTE: The HOM60120M200PC and HOM60120L225PC both come with covers that DO NOT contain a door. Also, please keep in mind the QOCDK60 is ONLY a box top type of door that is ONLY suppose to attach to the front cover on the load centers and go over the deadfront area ONLY, where the branch breaker handles show.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings