Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the Wire Retainer for the Coupling used on RWT Wall duct?
Issue:
Replacement for the wire retainer for the RWT wall duct

Product Line:
Wall Duct

Environment:
Installation

Cause:
Additional retainers may be required.

Resolution:
The wire retainer comes standard with the coupling device. If additional retainers are required, order as part number 4520660501.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings