Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is an isolated neutral available for 225A NQ panelboards?
Issue:
Isolated neutral for 225A NQ Panel

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1

Cause:
The NEC requires the neutral of a panelboard to be isolated from ground except when the panelboard is the service equipment.

Resolution:
An isolated neutral is provided as standard. A bonding strap is supplied in the hardware bag assembly for use when required.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings