Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What happens to Powerlink ECB breakers in the event of a power loss?
Issue:
What happens to Powerlink ECB breakers in the event of a power loss?

Product Line:
Powerlink G3 Lighting Control

Environment:
Commercial Lighitng Control in North America

Cause:

Resolution:
If a Primary Panel (Panel with the Powerlink Controller) loses power, then the breakers remain in the state that they were last commanded when the panelboard lost power.   The entire Powerlink subnetwork of secondary panels remain in the last state the breakers were commanded as well.

If a secondary Panel loses power, the breakers remain in the state that they were last commanded at the time the panelboard lost power.

If a primary Panel loses power but the secondary Panel does not, the breakers of the secondary Panel will all stay in the state they were last commanded.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings