Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the resistance on NEMA size 3, 2 & 3 pole, AC coils?
Issue:
What is the resistance on NEMA size 3, 2 & 3 pole, AC coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature (60 Hz only):

24V = 0.35 Ohms

120V = 8.48 Ohms

208V = 28.7 Ohms

240V = 34.1 Ohms

277V = 49 Ohms

380V = 85 Ohms

480V = 138 Ohms

600V = 261 Ohms

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings