Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does Ecostruxure Machine Expert Basic (Formally SoMachine Basic) support READ_VAR/WRITE_VAR Functions?

Article available in these languages: Spanish

Yes, as of SoMachine Basic version 1.3. Patch 1 now called Ecostruxure Machine Expert Basic.
Properties
Double-click on the function block to open the function properties table.
The %READ_VAR function block has the following properties:
Property
Value
Description
Used
Activated / deactivated checkbox
Indicates whether the address is in use.
Address
%READ_VARi, where i is from 0 to the number of objects available on this logic controller
i is the instance identifier. For the maximum number of instances, refer to Maximum Number of Objects table.
Symbol
User-defined text
The symbol uniquely identifies this object. For details, refer to the SoMachine Basic Operating Guide (Defining and Using Symbols).
Link
  • SL1: Serial 1
  • SL2: Serial 2
  • ETH1: Ethernet
Port selection
NOTE: SL2 and ETH1 embedded communication ports are available on certain controller references only.
Id
This parameter depends on the link configuration:
  • 1...247 for serial lines server address
  • 1...16 for Ethernet index
Device identifier
For more details about the Ethernet index, refer to Adding Remote Servers.
Timeout
The unit is in ms, with a default of 100.
A value of 0 means no timeout enforced.
The timeout sets the maximum time to wait to receive an answer.
If the timeout expires, the exchange terminates in error with an error code (CommError = 01 hex). If the system receives a response after the timeout expiration, this response is ignored.
NOTE: The timeout set on the function block overrides the value configured into SoMachine Basic configuration screens (Modbus TCP Configuration and Serial Line Configuration).
ObjType
The type of objects to read:
  • %MW (Mbs Fct 3): memory words (default)
  • %I (Mbs Fct 2): input bits
  • %Q (Mbs Fct 1): output bits
  • %IW (Mbs Fct 4): input words
The types of Modbus read function codes are:
  • Mbs Fct 3: equivalent to Modbus function code 03
  • Mbs Fct 2: equivalent to Modbus function code 02
  • Mbs Fct 1: equivalent to Modbus function code 01
  • Mbs Fct 4: equivalent to Modbus function code 04
FirstObj
0...65535
Address of the first object to read.
Quantity
  • 0...124 for %MW
  • 0...127 for %I
  • 0...127 for %Q
  • 0...124 for %IW
Number of objects to read
IndexData
0...65535
The first address of the word table to which read values are stored (%MW).
Comment
User-defined text
A comment to associate with this object.



If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings