Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU366DS, series E5 (or E05)?
The following parts are field replaceable:

Line base assembly - 4055218651 (3 required; includes arc suppressor assembly)
Line base mounting screws - 4020600901 (2 required per base)
Arc Suppressor Assembly - 4051270850  (1 per pole required)
Arc Suppressor mounting screw -  2140910321 (1 per assembly)
Line Base phase insulator - 4055219301 (2 required)
Handle Assembly - 4051219151
Handle Assembly mounting screws and washers - 2140122242 (screw; 2 required) and 2370100220 (washer; 2 required)
Handle Knob Kit - 4028343550 (includes the black and red parts with mounting screws)
Cross Bar Insulators - 4055217701 (2 required)
Dust Shield - 4055215701 (1 required)
Cross Bar Insulator - 4055217801 (1 required)
Main Lugs ONLY - 4405044601 (4 per pole or base assembly)
Main lug mounting screw and nut - 2140128481 (1/2-13 screw; 1 per lug) and 2342702800 (keps nut; 1 per lug)
Door Closing Thumb Screw and Retainer - S1A99898 (screw; 2 required) and 4405043301(retainer; 2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings