Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is used for a blank for top cable opening in a SA26PS?
Issue:
Closing plate for Speed D board underground pull section

Product Line:
Switchboards

Environment:
Speed-D

Resolution:
The SA26PS and SA26PSR, Nema 1 and Nema 3R Speedy SWBD Pull sections DO NOT come with standard side covers.

Side covers are normally associated to a switchboard, and the switchboard has side covers on both sides (please reference the Speed-D instruction bulletin).
The SA26PS and SA26PSR Pull sections only come with the metal wire way barrier (has an opening in the top for pulling cable through the pull section to the switchboard.
If there is a wish to use an SA26PS or SA26PSR as "stand alone" Pull sections, side covers MUST be ordered separately as part number 80370-004-02 (indoor side cover - requires (2) per side) 80370-025-01 (N3R side cover - requires (1) per side).
There is not a cover plate that goes over that wireway opening. It must be replaced with a side cover.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings