Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of punch is used for the HVIR windows?
Issue:
Part number for the punch used for the HVIR windows

Product Line:
Infrared comet windows

Environment:
HVIR Infrared comet windows

Cause:
Installation and maintenance

Resolution:
The Greenlee punches are used to punch to create the opening for the windows. These will need to be purchased from the local Square D/Schneider Electric distributors.
For 2 inch window use 730BB-2-3/4
For 3 inch window use 739BB
For 4 inch window use 742BB

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings