Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the sockets for RE48 relays?
Issue:
Looking for the sockets for the RE48 timers

Product Line:
Relays and Timers

Environment:
Zelio RE48 Panel Mount Timers

Resolution:
The socket selection is as follows:
IP20 sockets with connection by connector and mixed contact terminals
8 pin RE48ATM12MW or RE48AMH13MW  -  RUZC2M
11 pin RE48ACV12MW or RE48AML12MW  -  RUZC3M

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings