Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are there 3 position mushroom head operators in the current line like the old XB2BN operators?
Issue:
Are there 3 position mushroom head operators in the current line like the old XB2BN operators?

Product Line:
22mm operators - GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
No, this type of operator was discontinued after the XB2 product line.  The only current replacement would be a three position selector switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings