Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are alternate lugs available for the EZM31200GCBU and EZM31200JCBU Main Devices?
ISSUE:
Alternate Lugs

PRODUCT LINE:
EZM Metering

ENVIRONMENT:
Alternate Lugs

CAUSE:
Change in Wire Size

RESOLUTION:
Yes, alternate lugs are available for these devices, see the attached CAD drawing #PWFDS-SYTI-0028. BUT to use ANY of the lugs in the table on the attached CAD drawing the Utility Lug Landing KIT part number EZM1200ULL MUST be obtained.

The Standard Lugs provided on the EZM31200GCBU and EZM31200JCBU will accept (4) 3/0 AWG - 500 kcmil AL/CU per phase and Neutral.

Schneider Electric USA

Attachment(s)
PWFDS-SYTI-0028.pdf [137.51 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings