Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you set up the ATV212 drive using the VW3A1101 keypad as a multipoint access point using four drives and one HMI?

Issue:
Is it possible to set up the ATV212 drive using the VW3A1101 keypad as a multipoint access with four drives and one HMI?

Resolution:
The ATV212 does not support Multipoint or Multidrop access by connecting multiple drives to one HMI.

***

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings