Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between TVS3DSPHIC and TVS3DSPHC?
Issue:
Product Features

Product line:
Surge Protection

Environment:
UL 1449 3rd ed., ANSI/IEEE C62.41 and C62.45

Cause:
Understanding the difference between two similar part numbers may prevent a misapplication.

Resolution:
The TVS3DSPHC is a display that is horizontal (wider than it is tall) and goes into panels, switchboards, and switchgear.   The TVS3DSPHIC is vertically oriented (taller than it is wide) and is only for I-Line internally mounted SPDs.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings