Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a barrier kit available to prevent accidental contact with the SDGT30020, SDGT300300, SDGT300C10C or SDGT300C300C Auxiliary Gutter Tap Kits?
Issue:
Selection

Product Line:
Load Center Accessory

Resolution:
No optional barrier kit is available. The cover of the Auxiliary Gutter SDAG26 should not be removed unless power feeding the device is deenergized. This is noted on the WARNING label attached to the front cover of the SDAG26.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings