Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
MH68WP: What is the part number for the piece that the latch goes into?
Issue:
What is the part number for the door latch receptacle on a MH68WP panel can?

Product Line:
Panel Board

Environment:
NQ and NF

Resolution:
The black plastic piece that snaps into the side gutter cover to plug the hole behind where the latch engages is 80106-344-01.  It looks kind of like an ash tray.  If the item is not loaded on EQM you will need to get a price and order it from the local sales office.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings