Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for a closing plate for an NQSFB4HJ sub- feed breaker kit?

Issue:
What
is the part number for a closing plate for an NQSFB4HJ subfeed breaker kit?
Replacement Parts

Product Line:
NQ panelboards sold and supported in the USA.

Environment:
Maintenance

Cause:
Selection

Resolution:
The 2.3" x 5.5"  filler plate is a  80114-397-01 and it comes with rivets. This is the same filler plate used on the NQSFB2HJ and NF600SFBH.

Note: 80114-397-01  is an interplant part number. Please contact your Local Square D Sales Representative for more information.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings